Hi,
I am trying to get the Fs = 48kHz, SCLK = 32*Fs, MCLK = 256*Fs mode working, which is permitted for single-speed, software-controlled mode in the datasheet.
I am able to get all 3 clocks as expected, LRCK = 48 KHz, SCLK = 1.54 MHz and MCLK = 12.35 MHz. However, I keep getting the CLKE error (bit 3 in register 8). Also, I am not able to detect any output.
I have tried toggling the SPK-SD GPIO pin from high -> low -> high, but no change in result is observed.
When trying to toggle the SPK-SLEEP/ADR pin from high to low, I am not able to do so.
Has anyone faced such an issue? Can anyone help me with this?
Thank You.