Part Number: PCM4222
Other Parts Discussed in Thread: OPA1632, , , TPS65131, DIX4192
We have this elementary problem : we are using a PCM4222 with the exact OPA1632 input buffer as Texas is using in their evaluation board. One input of the OPA1632 is ou unbalanced RCA input, the other one is tied to Gnd. Our problem is that we can't get near 0dB full scale no matter how high is the level applied at the input. On the pdf we saw something confusing: for 0dB fs the adc requires 2.8v pp per input pin or 5.6v pp differential. The pdf also states that VCC is 4V and absolute max rating for VINL+ or VINL- is VCC + 0.3V. So, how should we measure those 5.6V pp differential ? We use a sine wave and a good Fluke 199C scopemeter... what are we doing wrong ? How should we consider "differential input" given that the swing per pin is +/- 1.4 V referred to the 1.95V DC offset ? Since both VINL - and VINL+ are using the same + 1.95 V DC offset (VCOM L)