Other Parts Discussed in Thread: TAS5766M
I have a Purpath Console Motherboard (AIP006G) along with a TAS5766MDCAEVM board that I'm trying to do some speaker tuning with. I recently used this same board setup with the same PC for tuning another speaker.about 1 week ago. It's been sitting in its ESD bag. I got it out do do some tuning on another speaker and I'm getting 2 error messages when running the hardware checks.
Error 1:Download Unsuccessful --> when I hover the mouse over the message, the popup contains "Check Whether the EVM is connected properly and re-run"
Error 2: Unable to playback audio --> the popup message contains: "Please check that you have not accidentally muted the EVM (or reduced volume to a lower level than maximum). If neither is the case, you may try disconnect and reconnect the EVM or rebooting your computer to fix this issue. If the issue persists, try with another EVM or post your issue on E2E. Please post a message on the E2E forums with your system configuration and any other relevant information.
The software connects to the TAS5766M EVM/Motherboard when starting the TS5766M app withing PPC3. When running the hardware checks, it never loses the connection.
System:
* Windows 10, version 1803 (OS Build 17134.1130)
* I verified that the EVM shows up in device manager and the sound control panel. I also verified the EVM is running: 2 channel, 16-bit, 48000Hz (DVD Quality)
It almost seems like the MCU on the motherboard got corrupted or something. Is there a way to program it manually so the "Download" passes?
Any other ideas?
Thanks,
David Smith