This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5121: PCM5121

Part Number: PCM5121

The figure is the parameters in the PCM5121 datasheet, please share the test conditions of these data. Such as Line out output impedance, output voltage or power, test circuit,  etc.

PCM5121 parameter:

DYNAMIC RANGE:106dB

SNR:106dB

THD:-92dB