This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The figure is the parameters in the PCM5121 datasheet, please share the test conditions of these data. Such as Line out output impedance, output voltage or power, test circuit, etc.
PCM5121 parameter:
DYNAMIC RANGE:106dB
SNR:106dB
THD:-92dB
Hi,
The output is stated to be -1dBFS of a nominally 2.1VRMS output. That means the output was 90% of 2.1VRMS.
Note (2) shows the the output load is 10kΩ to ground, but there is an additional 470Ω in series.
THanks,
Paul
Hi, the performance will be about the same if there is 10kΩ or no load. If you supply a -1dBFS input signal, then the output would be approximately 1.89VRMS.