This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Pls kindly help for below questions for DIR9001, thanks.
Thanks, Ian.
1. A phase-locked loop circuit attempts to synchronize to the incoming S/PDIF data stream and recover data and clock from it. If the PLL cannot lock, it cannot recover the clock and data. You don't switch between these two states -- PLL lock is a status based. Put simply, if the PLL does not lock, you cannot use the received data as they are not valid.
2. The S/PDIF decoder looks at status bits embedded in the recovered data stream (see the S/PDIF specification). EMPHASIS is used to indicate whether the audio data were encoded with a pre-emphasis filter. Also, S/PDIF can carry non-audio data packets. The AUDIO flag indicates whether it is receiving proper audio data or something else.
3. COUT and UOUT are channel status and user status bits derived from the decoder, and they are clocked out with LRCLK. If you need those status bits they are available.
4. CLKST is asserted when there is a change in PLL lock status. The data sheet tells you all about it.
5. What pins you need to connect to your system processor depends on your application. You might wish to re-read the data sheet.
Thanks Andy!
Ian,
I think Andy has you covered but let me know if you have any other questions!
Best,
Zak