Hello there, I was trying to understand how the output power of speaker can be set within Codec Control properly. There are some blocks (Analog attenuator and D-class Speaker driver ) which allows you to set some parameters in dB. Problem is that when I was set The Analog attenuator value to -6dB and output drive to +6dB I expected 0dB output amplification (the same like on Vin on input). This setting was working for headphone output (When I was set 0dB to both blocks the result was the same Vrms like on input Vin). I did another setting measurements (see excell attached) but I still don´t know the real transfr function between these numbers and functionality. My goal is to have real setting possibilities for setting the dB amplification/ attenuation. Than maybe something like logarithmic scale from 0 to 100% of full output power.
Thank Youscaling_1.xlsx