Part Number: OPA1654
Hi Team,
Please help confirm OPA1654 circuit,When OPA1654 has not been Powered-ON, I tested it.
The undesirable phenomenon measured is: The DC resistance value of the IC's PIN4 to PIN11 is abnormal when measured with a multimeter. The normal value is about 220K. Test the IC's PIN4 to PIN11 DC resistance on the PCBA. If the value is abnormal, I will remove it and measure it separately. Now the IC removed from the PCBA is tested separately for the DC resistance values of PIN4 to PIN11:
1. 61Ω
2. 2Ω
3. 3Ω
4. 3Ω
5. 2Ω
6. 267Ω
7. 205Ω
8. 281Ω