• TLV320AIC3106-Q1: Does the TLV320AIC3106 support a -23 dB gain depth with its two Biquad filters?

    Part Number: TLV320AIC3106-Q1

    Tool/software:

    Hello, TI experts, 

    We have received a requirement stating that each audio source should adjust the frequency response. Therefore, we would like to use the AIC3106 BQ1 and BQ2 to achieve this.

    However, we…

  • TLV320AIC3106: There is no sound problem. I need help checking the register

    Part Number: TLV320AIC3106

    Tool/software:

    Master chip provides 2.048m clock to codec mclk and pcm_clk sample rate 8k, hardware design right channel, codec horn, no sound Want to see if there is a problem with the accessory register?  If there is a problem…

  • TLV320AIC3106: Codec choice for AGC, noise cancelling and Echo Cancellation for Sitara AM437x Architecture

    Part Number: TLV320AIC3106
    Other Parts Discussed in Thread: TAC5212

    Tool/software:

    We are currently using TLV320AIC3106 codec on Sitara AM437x architecture and using SDK.05.02.00.10.

    I have two questions.

    Q1. Do you have suggestion on a different codec…

  • TLV320AIC3106: [ADC] Request for AIC3106 Codec Mux Routing Table

    Part Number: TLV320AIC3106

    Tool/software:

    Hi Team,

    The MIC BIAS voltage (2.2V) on the TLV320AIC3106 is now active based on AIC3106 datasheet table 10-33.

    https://www.ti.com/tw/lit/gpn/tlv320aic3106

    The current progress is that PCM is functioning, and…

  • TLV320AIC3106: Please help to review schematic of TLV320AIC316 working with TS3A227ERVAR.

    Part Number: TLV320AIC3106

    Tool/software:

    Hi Sirs

    Please help to review schematic of TLV320AIC316 working with TS3A227ERVAR.

    The purpose of using TS3A227ERVAR is that we want to use 4 different keys function, and also 4-pole Standard/OMTP Headset distinguished…

  • TLV320AIC3106: AIC3106 Bass and Treble adjustment

    Part Number: TLV320AIC3106

    Tool/software:

    Hello, I have a few questions about bass and treble adjustment,

    If I first set the bass to 100Hz(Fc), the amplitude gain is 1 dB, and then set the treble to 10KHz(Fc), the amplitude gain is 1 dB.

    1. Will the…

  • TLV320AIC3106: using "snd_soc_component_write" from an application

    Part Number: TLV320AIC3106

    Tool/software:

    since the 3106 codec driver doesn't have support for the DMIC or the page 1 filter parameters i need to be able to access registers directly. i was told in another post i can use "snd_soc_component_write" to…

  • TLV320AIC3106: unable to build driver with DMIC support

    Part Number: TLV320AIC3106

    Tool/software:

    in the related thread i was provided altered driver files that gave DMIC support. unfortunately i wasn't able to test it for some time due to prototype woe's. 

    i am finally getting to test it and i am…

  • TLV320AIC3106: Configuring AGC Function During Recording

    Part Number: TLV320AIC3106
    Other Parts Discussed in Thread: AM4378,

    Tool/software:

    We are using the TLV320AIC3106 Codec in our design, the OS is TI Linux (Linaro tool chain, Arago package) on an AM4378 microprocessor and are trying to configure the specific…

  • [FAQ] TLV320AIC3104EVM-K: When testing TLV320AIC3104EVM-K preset configuration, what do I do when AC-MODEVM Controller board is used?

    Part Number: TLV320AIC3104EVM-K
    Other Parts Discussed in Thread: TLV320AIC3105, TLV320AIC3106, TLV320AIC3107, TLV320AIC3101, TLV320AIC34, TLV320AIC3104

    Tool/software:

    If you are testing the EVM of TLV320AIC3104, TLV320AIC3101, TLV320AIC3105, TLV320AIC3106…

  • TLV320AIC3106: ESD protection for microphone inputs

    Part Number: TLV320AIC3106

    Tool/software:

    The 3106 datasheet says it has ESD protection up to 1.9kV (or 1.5kV depending on which ESD module you use for testing).  I assume that applies to all pins on the device.  If I wanted to add more ESD protection…

  • TLV320AIC3106: mono_lout audio setting inquiry

    Part Number: TLV320AIC3106

    Tool/software:

    hello.

    I have posted an inquiry using the link below, but I would like to ask if there is anything that needs to be modified in the settings.

    e2e.ti.com/.../5203902

    As in the title, I want a part with MONO_LOUT…

  • TLV320AIC3106: Not connecting MCLK

    Part Number: TLV320AIC3106

    We require that the 3106 be configured as the slave.  The processor will be the master of the audio bus, in this case a Renesas RZ/G2L processor.

    Section 10.3.3.1 of the 3106 datasheet implies that all internal clocking can be…

  • TLV320AIC3106: Missing AVDD_ADC pin

    Part Number: TLV320AIC3106

    The datasheet block diagram shows AVDD_ADC and AVSS_ADC pins, but there is no pin listed in the pin list for AVDD_ADC?

  • TLV320AIC3106: band pass filter for audio

    Part Number: TPA2012D2

    Hello Ti,
    I am using TLV320AIC3106IRGZT and TPA2012D2RTJR, but getting very high noise,

    can you suggest audio filter ( using LC or RC) to be implemted between TLV320AIC3106IRGZTTLV320AIC3106IRGZT and TPA2012D2RTJR.

    Regards
    Abhineet…

  • TLV320AIC3109-Q1: the driver of tlv320aic3109

    Part Number: TLV320AIC3109-Q1
    Other Parts Discussed in Thread: TDA4VM, TLV320AIC33, TLV320AIC3007, TLV320AIC3106, TLV320AIC3104, TLV320AIC3100, TLV320AIC3110, TLV320AIC3120, TLV320AIC3111, TLV320DAC3100, TLV320DAC3101

    Hi,TI

         Now we are debugging tlv320aic3109…

  • TPA2012D2: Noise in audio

    Part Number: TPA2012D2
    Other Parts Discussed in Thread: TLV320AIC3106

    Hello,

    I have connected the TPA2012D2 to TLV320AIC3106 via a low pass filter of nearly 30khz. I am using single-ended line mux.  Thier is a constant noise in it. Can you suggest any thing…

  • TPA2012D2: What is the operating frequency range?

    Part Number: TPA2012D2
    Other Parts Discussed in Thread: TLV320AIC3106

    Is the output signal of TLV320AIC3106 comes under the operating frequency range of TPA2012D2. 

  • TLV320AIC3106: Connection of MICDET in TLV320AIC3106 to TS3A227ERVAR

    Part Number: TLV320AIC3106
    Other Parts Discussed in Thread: TS3A227E

    Hi

    I am designing Audio circuit, and I plan to use TLV320AIC3106 as codec with TS3A227ERVAR as detection.

    here are the few questions

    1. It is supposed to get low level on MIC_Detection when…

  • TLV320AIC3106: Output Common-Mode adjustment not working

    Part Number: TLV320AIC3106

    Hello all,

    We are using a TLV320AIC3106 in an scenario where we adjust the levels of a microphone signal received in LINE1LP pin (in signle-ended mode) and we output it through LEFT_LOP.

    We have recently realized the signals…

  • TLV320AIC3106: How do i enable and use the digital Mic in linux?

    Part Number: TLV320AIC3106
    Other Parts Discussed in Thread: SYSBIOS

    we have a design that is using a digital mic but i am not seeing anywhere in the DTS documentation anything that indicates the use of digital mic

    https://www.kernel.org/doc/Documentation…

  • TLV320AIC3106: Power consumption assessment

    Part Number: TLV320AIC3106

    Hi Team,

    My customer wanted to evaluate the power consumption of the AIC3106, but the specification gave multiple reference standards.

    Can you help confirm which standard customers should refer to? And how do I determine the…

  • TLV320AIC3106: EVM DSN file

    Part Number: TLV320AIC3106

    Hi,

    Is possible to provide TLV320AIC3106 EVM DSN file to customer?

    Or can send mail to me Jeff YC Yang <JeffYC.Yang@arrow.com>

    Thanks!

    Jeff

  • TLV320AIC3106: #TLV320AIC3106IRGZR #Audio Codec #Right channel not working

    Part Number: TLV320AIC3106

    Hi,

    We are using TLV320AIC3106IRGZR in our custom board.

    Through I2S sending the audio and getting the speaker output only on LEFT OP and LEFT OM but not able to get anything on the RIGHT OP and RIGHT OM channel.

    Attached is…

  • TLV320AIC3106: 1x audio out, 1x microphone, and 1x stereo line in

    Part Number: TLV320AIC3106

    Hi,

    The customer specifies that the input/output for this codec is a 3.5mm 4-pole TRRS connector.

    However, to achieve the functionality of "1x audio out, 1x microphone, and 1x stereo line in":

    (1) Is it feasible? …

1 2 3 4 5 »