Dear TI Experts,
As we can see in datasheet, Output skew is 20ps, maximum of Part-to-part skew is 600ps.
Could you kindly tell me what is CDCLVD1213’s maximum skew out of all channel in single device under worst cases? Is it 20ps just the same as Output skew ?
Another question is if we don't make frequency divided with QDP/QDN , and combine other 3 channels. Is the maximum skewall of 4 channels 20ps?
Thanks a lot.
Comments from datasheet:
(1) Output skew is calculated as the greater of the following: As the difference between the fastest and the slowest tPLHn
or the difference between the fastest and the slowest tPHLn (n = 0, 1, 2).
(2) Part-to-part skew is calculated as the greater of the following: As the difference between the fastest and the slowest
tPLHn or the difference between the fastest and the slowest tPHLn across multiple devices (n = 0, 1, 2).