Hi Experts,
LMK61E2 has reserved bits in its registers. Most reserved bits have the same default value of 0, a few have the value of 1, e.g. R35.[1:0]. If we execute a I2C communication and use a byte to overwrite a specific writeable register, how should we make the bit value which is in same position in the byte as the one in the register, the default value or any value?
The datasheet mentions little on the XO Margining Offset Value(R16 and R17) . The LMK61xx Oscillator Programming Tool has a input entry to modify the load capacitor value. What is the upper/lower bound of the XO_CAPCTRL value, 0~2047? Do you have any formula to correlate this XO_CAPCTRL value and the offset of out frequency? Do we need a spectrum analyzer to verify such frequency fine turning does happen?
Best Regards!
Wallace