Hi,
How much is driving current capacity of DRVn pin?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kuramochi,
According to datasheet section 6.6, rise time of DRVn pin with 50pF load is 50ns. Based on EC table test conditions, VDD = 2.5V. For 20% to 80% rise time, V = I/C * t, so current = 2.5*0.6 * 50e-12 / 50e-9 = 1.5mA.
Regards,
Hao