Other Parts Discussed in Thread: LMK04828
Dear colleague,
Our customer has below concerns:
1. When using external VCO mode (J6), after loading the file lmk_config_external_clock. CFG, both PLL1 and PLL2 lock status lights are off. Is PLL not working or external VCO mode is not using PLL? Doesn't the high-speed sampling clock output to ADC require octave?
2. If PLL is not used, does the external input clock source need high frequency? But I see that the input range of Fin in the datasheet is 0.001~750MHz, so how to understand it.
Best Regards,
Rock Su