Hi Team,
Need some clarifications on LMK03318 single-ended outputs. In section 7 (pin configurations), the pin function of clock outputs 0-7 are described as: “Differential/LVCMOS output pair. Programmable driver with differential or 2 x 1.8V LVCMOS outputs.” Is this saying that the LVCMMOS outputs can only be configured for a voltage level of 1.8V?
Our customer wants the voltage level of the single ended LVCMOS output clocks to be 2.5V. Other places in the datasheet says the outputs can be 2.5V, but this pin description somewhat gives confusion. Can you help us clarify?
Kind Regards,
Jejomar