Part Number: LMK04832
Other Parts Discussed in Thread: PLLATINUMSIM-SW
Hi,
I'm working on a Linux driver for the lmk04832, and so far the clock distribution is mostly supported.
I'm now having issues synchronizing the device clocks to the sysref to be able to support JESD204B subclass 1.
- What is the shortest sequence to re-synchronize the device clock to the sysref? is everything in section 8.3.2?
- Do I have to manually set the DDLY values or is that done automatically during a synchronization sequence?
- Should a re-synchronization be triggered each time the SCLK rate is updated?
Thanks for your help,
Liam