Other Parts Discussed in Thread: LMK03328, TICSPRO-SW
Hi Teams,
Our customers require…
Input: 27MHz, H/V/FID
Output 1: 148.35MHz or 148.5MHz(for Camera head transmission)
Output 2: 148.35MHz or 148.5MHz or 54MHz or 297 MHz or 296.7 MHz (refclk for HDMI channels)
Output 3: 148.35MHz or 148.5MHz or 74.25MHz or 74.175MHz or 54MHz or 297 MHz or 296.7 MHz (refclk for HDMI channels)
HDMI 1: 2160p59.94/50 2160p29.97/25
HDMI 2: 2160p59.94/50 2160p29.97/25
1080p59.94/50 1080psF29.97/25
How can our customers design such systems?
Do you have some ideas to circuit construction of this system with LMH1983 and LMK03328 or other CLK Gen.?
Our customers will need to know whether these CLKouts can be implemented or not.
If possible, would you teach me how to implement theseCLKouts with LMH1983 or other CLK Gen.?
Best Regards,
Maki