Other Parts Discussed in Thread: LMX2592
Has anyone used the MUTE pin to switch between synthesizers? I want to ping pong two LMX2820's and think I may be able to save a switch by tying two outputs together and only enabling one synth at a time with the MUTE pin. I am using it around 6 GHz so of course impedance is an issue. What do the outputs look like? The datasheet says there is a 50 ohm pullup- is that still there when the output is muted? Any experience with the best way to do this? I could use a splitter to combine them, but has anyone used something simpler like a resistive split?
BTW- Lock times look very nice with the instant cal- very good idea, wish your lower freq PLL parts (e.g. LMX2592) had this feature.
Thanks