This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
My customer evaluating the DAC34H84EVM with the DAC348x EVM Software GUI. They want to set LVDS clock output as 207.36MHz from J10/J11 pins of the DAC34H84EVM which are U4P/U4N pins of the CDCE62005. The DAC34H84EVM has the 19.2MHz TCXO which is inputted into SEC REF+ pin of the CDCE62005.
They set the GUI as attached, but they got 211.29MHz LVDC clock output from J10/J11 pins of the DAC34H84EVM.
Could you advise them on how to set up the GUI to get the correct 207.36MHz LVDC clock output from J10/J11 pins of the DAC34H84EVM?
CDCE Output Settings, Y4 FPGACLK2 is settings for J10/J11 pins of the DAC34H84EVM.
I look forward to your reply.
Thank you.
Best Regards,
Koshi Ninomiya
Hi Koshi,
I'm not familiar with the DAC GUI (not even the clock part of it). Can you reach out to the DAC team instead?
Regards,
Hao