Other Parts Discussed in Thread: CDCE62005, LMK03806, CDCM6208
Dear All ,
I am using CDCE62005 chip in my custom board. i would liek to generate the following clock outputs . All are LVDS differential signals . I am using a 25 MHz crystal. The PRI_REF and SEC_REF signals are unconnected.
Output 0 - 100 MHz
Output 1 - 312.5 MHz
Output 2 - 312.5 MHz
Output 3- 125 MHz
Output 4 - 312.5 MHz
Can CDCE62005 generate the above set of outputs ? I tried to use the CDCE62005 EVM controller software and figured out that this is possible . However , the VCO is going OFF limits with this combination (shown in the fig below). Can anyone suggest an alternative scheme of generating the above set of clocks ?

-Anil