Other Parts Discussed in Thread: LMX2492
Hello,
I am trying to use two LMX2492EVM to build a simple RF TX and RX system. Attached are the system setup.
On the first board, only PLL (U1: LMX2492) is used. The VCO (U2:MACO-009265) is not used (R4 is disconnected and no Vtune to U2). The RX antenna's signal feed back PLL's Fin* signal. The R6, which connect the on-board VCO output, is removed.
On the second board, only VCO is used (R4 is disconnected). The Vtune is connected by a wire from the 1st board to the 2nd board. The TX antenna is transmitting RF signal.
The idea is simple: 1st board receives RF signal to drive Vtune. The 2nd board receives Vtune to drive VCO to transmit RF signal. The two boards share the same 5V and ground. The setup is similar to the single LMX2492EVM board, except now the RF TX (by VCO) and RF RX (by PLL) are separated into two boards.
To our surprise, the PLL can only lock (by monitoring MUXOut LED) around 9.1GHz. And the lock is not solid (LED blinking, instead of solid on). In the single board system, the PLL can lock from 9.1GHz to about 10GHz. The LED is solid on.
Please help us to understand this behavior. This is the first step to use the LMX2492 in a real TX/RX setup. The LMX2492EVM uses the on-board trace of Fin to feedback, not through the SMA antenna.
Thanks a lot for the help.
Yuke