Other Parts Discussed in Thread: LMK05028
Hi Teams,
My customer want to operate the LMK05028EVM in 2 loop mode which only enable the reference inputs and XO.
(They will use OCXO to replace XO in final design.)
Q1. When they are evaluating EVM performance, they found that only input is 25MHz which is default setting of EVM recommended can sync the output signal with input signal, but change the input frequency will not be able to sync, and D12/D13 will light up which means input/output are not sync.
Q2. About the phase noise, they are wondering which is better between 2 loop/3 loop mode? Because they intend to use 2 loop mode.
Thanks.