This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2492: control high voltage Vtune VCO

Part Number: LMX2492

Hi Texas Instruments,

I want to make 11GHz output on LMX2492 and external VCO, MAOC-009265-TR0500(VCO on LMX2492evm) or most of VCO on market have 12V Vtune, but CPout of LMX2492 is 5V. Therefore, I need an active loop filter.

I use Pllatinum Sim, there are 3 active filters are: type A, B, C.

1. Type A and B: have not AmpGain option, can I use type A or type B to control 12V Vtune VCO? 

I try this Schematic but it not working, Cpout connect CPout on LMX2492, Vtune connect Vtune of VCO

2. Also, I try type C with ampgain is 3(5V CPout x 3 = 15V Vtune), its not working again, can you help me?

here is my Schematic:

Where is my wrong?

Thank you!

Best Regards,

Ngandv