Part Number: LMX2492EVM
Other Parts Discussed in Thread: USB2ANY, CODELOADER, LMX2492
Hello every one.
I have a LMX2492EVM board, a USB2ANY and use TICS PRO to control it.
everything is ok with CW mode, the PLL can lock and DLD is OK。
It seems also OK with Ramp mode when "Start next ramp afer" whith "TOC Timeout", I think they run with free mode.
When I want to test trigger mod ,like use TRIG1_MUX PIN、 TRIG2_MUX PIN ,etc. to trigger LFMCW,but It is not work.
Also, I am according to the LMX2492EVM GUIDE.pdf section3.2.2 "Frequency Shift Keying (FSK) Example" to generate FSK , it is not wok too.
I thought the trigger signal is come from USB2ANY to uWire, but it seems no TTL tigger signal.
The firmware is 2.7.0.
In old userguid document, I see there are some signal allocation options in CodeLoader. but there is no similar options in TICS PRO, so I want to know how to comfirm the USB2ANY trigger signal is normal
thinks


the old CodeLoader.