Part Number: CDC7005-EVM
Other Parts Discussed in Thread: USB2ANY, CDC7005
Hi, I am trying to run this EVM and I am quite puzzled.
First the EVM interface is a parallel port but no cable (to USB or similar) is provided or indicated anywhere. I have seen the SPI signals are also easily accessible.
Second, the software that is supposed to be used to run this board is just causing an error in my Windows 10 - This application has requested the Runtime to terminate it in an unusual way- Any clue on this error?
Finally I have try to see if the TICS pro supports this board with the hope of making my own interface from the USB2Any and the CDC7005-EVM board, but it seems the board is not supported. So, how am I suppose to evaluate this board?