Hi Team,
Can you check for me, TI's SE555, is the OUTPUT driven is a voltage source or a current source?
I read the description in the manual, and it can output a maximum current of 200mA. I understand it means: voltage source, working according to the current demand of the load, and can output a maximum of 200mA. Is it right?
Because I connected a gate circuit in the rear stage, if it is a current source of 200mA, there is a risk, please help to evaluate it. Thank you so much.
B.R.
Lucas