This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828: Clock for THS5641A

Part Number: LMK04828
Other Parts Discussed in Thread: THS5641A

We are using LMK04828 to provide a clock for THS5641A.

LMK04828 doesn't seem to generate a 3.3V CMOS clock output, which I believe THS5641A is expecting.

I've summarized the issue in the attached pdf.

Could you suggest an output type and RC values to meet the digital input spec of THS5641A?

Thank you,

Andrewnotes 040323.pdf