Other Parts Discussed in Thread: LMX2492
Dear Texas team,
We want to synchronize two signal generators RF output. The signal is a LFM (chirp) signal. Can we use trigger input to synchronize both signal generators.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Texas team,
We want to synchronize two signal generators RF output. The signal is a LFM (chirp) signal. Can we use trigger input to synchronize both signal generators.
Hi Amit,
I assume you are saying frequency synchronization of two LMX2492.
We've never evaluated this application, you can try, with the following pre-conditions
1. both LMX devices should share the same reference clock
2. fpd = fosc. That is, R-divider = 1.
3. use a trigger signal to kick start frequency ramping.
Hi Amit,
You can setup RAMPx_NEXT_TRIG to use an external trigger source to kick start a ramp.
As far as I can remember, once the PLL receives the trigger signal, that particular ramp will get started immediately. However, I did not measure the actual delay time.