This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2581: harmonic outputs are hi and affecting my demod image rejection

Part Number: LMX2581

I am running differential outputs with 50 ohm pullups and driving into a demod chip that has input imped of 100 ohms. At 750M I'm measuring a high second harmonic level of -10dBc. I am only getting 18dB image rejection from the demod and I believe it is these harmonics that are creating the issue. Page 7 in the data sheet shows typical 2nd harmonic level of -25dBc. I'm using output A and output B is disabled. Is this performance to be expected? Is there anything I can do to reduce the harmonic content in the output? Would using the inductor give better harmonic performance? My system needs to tune from 740 to 2400M.