This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We're trying to analyze the phase noise of our LMK5B33216EVM board. We're using an SIT5347AE-FN-33E0B100.000000 MEMS oscillator, producing a 100 MHz signal, which is connected to the Y3 blueprint on the evaluation board:
We're producing a 156.25 MHz output, using only APLL3 (DPLL disabled), with these settings in TICS PRO:
However, when measuring the phase noise with our E5052B signal source analyzer, we observe a larger RMS jitter than expected when compared to the datasheet (with noticeable spurs at higher frequencies, far outside the loop filter bandwidth):
Could you advise us on what may be the source of our issue - in particular, the high frequency spurs? Thank you in advance!
Best,
Joel
Hi,
Do you have intention of using the DPLL? If not, configure APLL3 more optimally to have 100 MHz phase detector frequency.
Note default settings are which I would suggest for the charge pump and loop filter values.
If you want to use DPLL, you should have a non-integer relationship between XO and VCO frequency for DPLL to be able to avoid integer boundary spurs. This is not true with the 100 MHz direct, however it appears you were aware of this and configured for *2 /3 so that 2500 MHz / 66.66 = 37.5. This does indeed avoid the integer boundary, although there may be some 2nd order effects.
Do you have other clocks operating at different frequencies close-by which could be crosstalking?
Were you able to remove power from the primary TCXO for EVM? You should have only on XO powered. See info below:
Oscillator Designator |
Example Part Number |
Type, Package |
Power Resistor |
Localized 0.1 uF bypass |
RF output resistor |
Y1 |
7N48071001 |
Common 7.0 mm x 5.0 mm, 4 or 10 pin |
R206 |
C80 |
R43 |
Y2 |
8W48072003 |
Common 2.5 mm x 2.0 mm, 4 pin |
R207 |
C82 |
R46 |
Y3 |
7X-50.000MBB-T |
Common 3.2 mm x 2.5 mm, 4 pin |
R208 |
C83 |
R47 |
Y4 |
ROM9070PA |
OCXO, 9.7 mm x 7.5 mm, 4 pin |
R209 |
C84 |
R48 |
Y5 |
ROX2522S4 |
OCXO, 25.4 mm x 22 mm, 7 pin |
R210 |
C85 |
R49 |
73,
Timothy
Hi Timothy,
Thank you for the prompt response! We do intend to use the DPLL eventually, which is why we chose those parameters to avoid the integer boundary.
I tried adjusting the values of R3 and R4 as well as unchecking PLL3_CP_PU_DIS, but I still see an RMS jitter of around 115 fs with the high frequency spurs in the phase noise plot. Also, I don't believe we have any other active clocks or XOs on the board that may be interfering with our MEMS oscillator or APLL3 output.
We plan to test our setup using a new LMK5B33216EVM board without any modifications, just to compare against our board with the MEMS oscillator and to verify that our lab setup (power supply, phase noise analyzer, etc.) is correct. We'll keep you updated if we can locate the source of our high jitter and spurs - thank you again!
73,
Joel
Hi Joel,
I checked with your TICS Pro settings with 100 MHz from sig gen SMB100A and did not observe that high rms jitter on the output. Let us know if your new board could get better PN.
-Riley
Hi Timothy and Riley,
Thank you again for your feedback on this question. We realized that we were using OUT0 for our output, which is DC-coupled. We switched to OUT4 to generate an HSDS signal, and now we're getting an RMS jitter of ~53 fs for both evaluation boards, which is much closer to our expectations. Thank you again for the assistance - we really appreciate it!
Cheers,
Joel