This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2572: FSK Deviation (MHz) with high PLL_DEN

Part Number: LMX2572

Hello,

We like to use the PLL LMX2572 in FSK mode. We use the software TICS Pro in order to configure the eval board LMX2572EVM.

We want to program a jump of order of MHz around a fixed frequency.

Following the equation given in the LMX2572 datasheet (equations 9 & 10 p73), we succeed to have those jumps with quite small PLL_DEN (<100M) but with higher values it does not work.

We don't see any limitation on the LMX2572 datasheet.

Here are our PLL configuration in TICS PRO in order to reproduce the problem:

  • OSN_IN = 100MHz
  • Fpd = 100MHz
  • PLL_N = 60
  • PLL_DEN = 4294967295
  • PLL_NUM = 0
  • PFD_DLY_SEL = 5
  • MASH_ORDER = 4th Order Modulator
  • MASH_RESET_N = enable
  • Fvco & RFoutA = 6GHz
  • Output MUX A = VCO
  • FSK_DEV_SCALE = 13
  •  FSK_SPI_FAST_DEV = 1311
  • FSK_MODE_SEL = FSK_SPI_FAST
  • FSK_EN = enable

Is there a reason why we can't observe a deviation of MHz when we have a high PLL_DEN ?

Thanks in advance for your answers.

Best regards,

Malo