Other Parts Discussed in Thread: ADC09DJ1300, LMK04832
Hello,
Currently I try to connect SYSREF+/- differenctial pair of LMK04828 to that of ADC09DJ1300.
I am thinking of using DC coupling of LVPECL interface because of JESD204B interface. But I am not sure how to do that with the condition which power supply of both LMK04828 and ADC09DJ1300 are 1.8 V.
I could find out some reference for DC coupling of LVPECL but their power supply are always either 3.3 V or 2.5 V and their Vtt (termination voltage) are Vdd - 2 V. So If I applied this to my design it would be minus voltage.
Is it possible to apply LVPECL interface with the condition which power supply is 1.8 V and DC coupling.
Thank you.