Part Number: LMX2594
Hi Team,
There is a section I didn't understand in the datasheet 7.3.13.2 describing the maximum slew rate of the automatic ramping must be kept less than 250kHz/us.

The example given 7.3.13.2.2 just below this section shows a 2GHz ramp within 2ms which is 2MHz/us by excluding the calibration time.

Is there an error or I'm missing something?
Thanks for your help,
BR,
XL