This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2595: What is the maximum slew rate of a calibration-free automatic ramp?

Part Number: LMX2595


Tool/software:

I am trying to generate an automatic ramp signal between 10.2 and 10.25 GHz over 5 microseconds with the LMX2595EVM.  However, when I configure the ramp parameters for this waveform, I am not able to generate the desired ramp signal.  However, if I change the ramp time from 5 us to 20 us, I am able to generate the desired signal.  What is the maximum ramp slew rate for the LMX2595?  It looks like 50 MHz over 5 us (10 MHz/us) exceeds this limit, while 50 MHz over 20 us (2.5 MHz/us) works.

Would it be possible to achieve a 50 MHz over 5 us (10MHz/us) ramp with the LMX2595 if I increase the bandwidth of the loop filter?