This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03328: I2C pull-ups with no power supplying

Part Number: LMK03328

Tool/software:

Hi support team,

Can I connect the I2C lines (SDA, SCL) of LMK03328 through pull-ups to a different power net than VDD_DIG when LMK03328 is no power supplied?

According to section 8.1 of the datasheet, the Abs Max of  SDA(#25) and SCL(#26) are 3.6V, which can be read as being independent of own VDD.

Is my understanding correct?

A further question: is there any problem with I2C access to devices at other slave addresses when that power is not supplied?

Best regards,