This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04803: LOS function details

Part Number: LMK04803

Tool/software:

Hi team,

This is FAE Jayden, my customer is using LMK04803BISQX, and they have some questions that need to reach out to you.

1)  As described in datasheet, Pin 62 and Pin 63 can be configured as  LOS status indictor. Device pin 62/63, Status_CLKin1, can be used as LOS status monitoring.

  1. Regarding the detection principle of loss of signal, or the detection window, can you help clarify under what specific conditions will the input signal be judged as lost? Are there clear indicator requirements for the amplitude, frequency deviation, and duration of signal loss of the input signal? 
  2. Regarding the signal amplitude, the datasheet currently gives the minimum differential input signal of 0.5Vpp. When the amplitude is less than what, an alarm will be reported? 

2) As for handover mode, If the input signal is lost, the output signal will be locked to the state before the signal was lost. Do we have corresponding data on the performance of long-term operation in this state? If it is kept in holdover mode for a long time, can the signal quality of the output signal be maintained? Will the output signal amplitude, frequency deviation and other indicators change over time? If the input signal does not appear again, will the holdover mode be maintained?

Brs

Jayden