This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCS504-Q1: Do we have any Clock Clock Buffer which support X2 Clock Multiplier?

Part Number: CDCS504-Q1
Other Parts Discussed in Thread: CDCE913

Tool/software:

Hi, Team

My customer needs the Clock Multiplier, and it seems the CDCS504 can only support "Frequency Multiplication Selectable Between x1 or x4 With One External Control Pin", but my customer needs x2."

My customer requirement, CLK input is 24.156M Hz, they needs the output is 24.156M*2=48.312M

Do we have any suitable device?

Thanks.

G.W

  • GW,

    How many outputs are they looking to have? The CDCE913 can be configured via EEPROM to function as an x2 multiplier for this input clock, with up to three copies of the clock.

    Thanks,
    Kadeem