Part Number: LMX2581E
Other Parts Discussed in Thread: CODELOADER
Tool/software:
Hello,
we use the LMX2581E in a Downconverter as Local Oscillator (LO). So far I can initialize the unit and set the frequency and the unit is operating well. The frequency will not changed so much so it could be that the chip will not reveive a new frequency setting over some weeks.
So far so good, now my problem. Sometimes after some days or weeks (without re-programming the frequency) the unit will lost the lock. A re-initialize and/or re-setting of the frequency will solve the problem. However a periodic initializing or re-setting of the frequency is not so nice since we lost the downconverted signal for a short time.
We have actual 4 prototype boards running and all of them show the same issue, so a expect that this would be a general problem.
We have two chips on each board, one is used in a
1) Wideband operation as intereger N configuration 1MHz stepsize from
- 1715MHz – 1900MHz, (3430-3800) VCO 4 divider 2
- 1900MHz – 2270MHz, VCO 1
- 2270MHz – 2720MHz, VCO 2
- 2720MHz – 3215MHz, VCO 3
2) Small band operation as fractional-N configuration 1khz stepsize from
- 695,04091MHz – 695,95000MHz (2780.16364-2783.8) , VCO 3 divider 4
So far we see the lock problem only in 1) wideband operation synthesizer.
Please find attache the schematic of synthesizer 1). OSC in = 50MHz

and the Settings of the register.
#define LO1_R5INIT 0x40870010 // Reset Chip to default settings, default from codeloader TI
#define LO1_R15 0x021FE80F // default from codeloader TI
#define LO1_R13 0x4082C10D // default from codeloader TI
#define LO1_R10 0x210050CA // default from docu TI
#define LO1_R9 0x03C7C039 // default from docu TI
#define LO1_R8 0x207DDBF8 // default from docu TI
#define LO1_R7 0x00000317 // default from codeloader TI
#define LO1_R6 0x000004C6 // default from codeloader TI
#define LO1_R5 0x00108005 // 0x00r08d05 d=0 OutputA is the VCO; r=1 fref<64MHz
#define LO1_R5DIV 0x00108805 // 0x00r08d05 d=8 OutputA Divider active, is set in R3 to 2; r=1 fref<64MHz
#define LO1_R4 0x00000004 // default from codeloader TI
#define LO1_R3 0x200002B3 // 0x20000gg3 gg = gain(0..47)*4+3; -2dB = 10*4+3 = 43 = 0x2B (Output PWR Off)
#define LO1_R2 0x0C000002 // 0x0Cddddd2 ddddd = PLL_DEN = 0 = 0x0000
#define LO1_R1 0xFE000321 // 0xFE000rr1 rr = RefDiv = 0x32 = 50 (VCO 4 Selected)
#define LO1_R0 0x68DA0000 // 0x6mmm0000 mmm = freq from 1880MHz to 3880MHz; default = 2266 = 0x8DA
// default for RFin = 1500MHz = LO= int(1500 + 765.5 + 0.5) == 2266 = 0x8DA
Is there are any recommandation, to improve that?
Best Regards
Klaus Schoenwald