Tool/software:
hello,
i ve some question about the output enable input from the LMK00105SQ.
should i connect the pin direct to vcc or with an 10k pullup resistior.
in the eval board the pin is direct connected.
thanks a lot
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
hello,
i ve some question about the output enable input from the LMK00105SQ.
should i connect the pin direct to vcc or with an 10k pullup resistior.
in the eval board the pin is direct connected.
thanks a lot
Hi Tee,
Both options are okay, but I would pull straight to VCC just board for ease.
One less passive component on layout.
Best regards,
Vicente