This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04828BEVM: PLL2 Lock

Part Number: LMK04828BEVM

Tool/software:

Clkin1: 122.88MHz/0dbm

EXTERNAL VCO: 122.88MHz

PLL2 does not LOCK.

The .txt file is also attached to the attached file. Please help me.

 

AFE_2457.6MHz_HSDS10mA_5.1M(2cycles).txt
Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
R0 (INIT) 0x000090
R0 0x000000
R2 0x000200
R3 0x000306
R4 0x0004D0
R5 0x00055B
R6 0x000600
R12 0x000C51
R13 0x000D04
R256 0x01000A
R257 0x010155
R258 0x010210
R259 0x010310
R260 0x010422
R261 0x010500
R262 0x010691
R263 0x010701
R264 0x010801
R265 0x010955
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX