This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC555-Q1: TLC555QDRQ1

Part Number: TLC555-Q1

Tool/software:

I want to design circuit with 2 seconds delay in output waveform change compared to input waveform change and I am considering using TLC555-Q1.

However, datasheet seems to assume input waveform is square waveform with constant frequency.

In my case, input waveform is always HIGH, drops to LOW when certain problem occurs and then recovers to HIGH again when problem is solved.

Under these input waveform conditions, is the TLC555-Q1 suitable for the purpose?

  • Hello Jiwon, welcome to the TI e2e forums.

    You have a very common request. I have seen the same request three times this week. In all three cases there was not a full description of desired behavior.

    Is it this list?

    1) High to low input causes a 2 second output. 

    2) Low to high input causes a 2 second output. 

    3) What should happen if the input changes while 2 seconds is still running?

    All input cases must be considered.

  • While it's true that those three requests are related, i don't think i've received a clear answer to my question.

    HIGH to LOW : no delay

    LOW to HIGH : 2 sec delay

    We assume no change in the input signal during the 2 second delay.

  • Jiwon,

    The output of this circuit goes low immediately when input goes low. For as long as input stays low, output never goes high. Once input goes high, the output remains low for 2 seconds, then output goes high. For cases where input is not high for at least 2 seconds then output always stays low. 

    N1 and N2 can be replaced with a logic buffer (or comparator) with open drain output. N3 an be replaced with a logic invertor.  

    TLC555 rising delay 2s.TSC