This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE913: Are the Y outputs symmetrical (50% duty cycle) at any divide ratio?

Part Number: CDCE913

Tool/software:

I would like a clarification.

The data sheet tells that the output duty cycle is symmetrical, nominal 50% duty cycle, with PDIV=1.

Is that still the case with other values of PDIV, or is the ODC varies with PDIV, as I would expect from most dividers?

Thank you very much