This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
We would like to know VOCM (Common Mode Output Voltage) , VOD(Differential output Voltage) ?
For VOD, We are setting Output Power Code (OUTx_POW) - 7.Based on the graph in the datasheet the corresponding dBm value is 3.5 dBm. When this dBm (3.5) is converted to voltage we are getting "0.94630" .Do we have to consider this value (0.94630) or multiply by 2*0.94630 =1.8926 as VOD ??
FYR I have attached an image from the datasheet. Let me know if you need anything else.
Hello,
Our expert for this device is out of office today. I've assigned this thread to them, please expect a response tomorrow.
Regards,
Connor
Hi Narender,
0.94V is the single-ended voltage swing we can measure at _P or _N pin.