This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
I have a few questions regarding LMK03318 and the evaluation board:
Thanks,
Prasoon
Prasoon,
1. The LVCMOS outputs will be 1.8V regardless of VDDO, however it is recommended to have the corresponding VDDO have 1.8V, if possible. If 3.3V LVCMOS outputs are needed, the STATUS pins can be used for that case.
2. A ferrite bead and bulk cap may be shared to supply multiple output banks with the same PLL/frequency. But we recommend each VDDO pin should have its own bypass cap.
3. Many of these 0 ohm resistors are placed to allow for more customization ability for the EVM.
4. The EVM has jumpers that can be populated and used for this [JP9-14]
5. Yes
6. Overall, yes, but see my answer to question 2.