Tool/software:
I need to match the output with a mixer, what's the output impedance on the synthesizer?
Also, I don't think it's possible, but I'll ask. Is it possible to get differential outputs from this chip?
I need a synthesizer that will work at at least -40-105C that has 0-1GHz range. If the LMX2571 had differential outputs, it would be perfect. Differential outputs would decrease the LO bleed through in the mixer.
Thanks,
-corey
Hi Corey,
We don't have the s-parameter of this device.
Outputs are not differential, they are two single-ended output with the same output phase.
We don't have many extended temperature devices. LMX2571-EP however is a single-ended output device. LMX2694-EP is differential, it can work up to 15GHz.