Part Number: LMX2820
Tool/software:
To perform Instant calibration in LMX2820EVM is it necessary to check VCO_CAPCTRL_FORCE, VCO_SEL_FORCE and VCO_DACISET_FORCE?
I performed the following steps
Initialization register setting
1. Set DBLBUF_PLL_EN, DBLBUF_CHDIV_EN, DBLBUF_OUTBUF_EN, DBLBUF_OUTMUX_EN = 1
2. Set DBLR_CAL_EN = 0; INSTCAL_SKIP_ACAL = 0
3. If VCO doubler is required, set INSTCAL_DBLR_EN = 1, otherwise set this bit to 0
4. Set INSTCAL_DLY = T x fosc (in MHz) / 2^CAL_CLK_DIV, where T = 2.5 x CBIASVCO / 0.47µF. CBIASVCO is the bypass capacitor at pin 3
5. Configure other registers to lock to 5.65GHz without any calibration assist
6. Set INSTCAL_PLL_NUM = 2^32 x (PLL_NUM / PLL_DEN)
Programming
7. Vcc power up LMX2820
8. Program all the registers, LMX2820 should lock to 5.65GHz
InstCal calibration
9. Program INSTCAL_EN = 1
9.5 run Index routine
10. Program R0 (with FCAL = 1), calibration will begin
11. Wait 100ms
12. Program R0 (with FCAL = 0) to complete the calibration
13. If LD pin did not turn HIGH, program RESET = 1 to reset LMX2820. After LMX2820 is reset, repeat Step 8 to 12
Changing VCO frequency
14. Program INSTCAL_PLL_NUM, PLL_N, PLL_NUM and PLL_DEN (if their value have change)
15. Program R0 (with FCAL = 0) to change VCO frequency
Yet my lock time is still 43.26us. Isn't it supposed to be 2.5us as mentioned in the datasheet?