Hi
General VCO I know needs more than 10V of voltage at 14GHz.
But Vcp of LMX2492 is Vcc (min) and 5.25V (max).
Vcc (for example, 3.3V) is low, so VCO of 14GHz can't be driven.
Do you know VCO where 14GHz can be output in LM2492?
If the circuit which amplifies the voltage of Vcp again is necessary, please tell me the circuit.
Best regards