Hi,
I would like to ask you a question about timer device.
What is the difference between LM555, NA555, NE555, SA555 and SE555?
LM555 SOIC-8 0~70 ℃ Tj:150℃
NA555 SOIC-8 -40~105℃ Tj:150℃
NE555 SOIC-8 0~70 ℃ Tj:150℃
SA555 SOIC-8 -40~85 ℃ Tj:150℃
SE555 SOIC-8 -55~125℃ Tj:150℃
The difference is just temperature?
Thank you in advance.
Best Regards,