Other Parts Discussed in Thread: LMK04821
Hi Team,
Please advise on the attached file.
Thanks,
Shlomi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMK04821
Hi Team,
Please advise on the attached file.
Thanks,
Shlomi
Hi Timothy,
LMK04821 schematic section is attached.
Please review.
Thanks,
Shlomi
Hello,
Power
You do not need to place separate ferrite bead for each clock group Vcc (Vcc#_CG#) if the clock output groups share the same frequency. It is acceptable but unnecessary. I do this for EVM because I don't know what frequencies will be on the outputs.
Inputs:
I presume that R466 will be placed closed to LMK IC.
Be aware of low impedance DC path to ground on CMOS output as is case for VCXO. I recommend not doing this as CMOS is typically designed for driving high impedance capacitive loads.
For CVHD-037X-100 VCXO which is 3.3 V CMOS, the OSCin is specified for 2.4 Vpp max SE. To achieve this I suggest adding a series resistor and cap to the output of X3. So Pin 4 --> 100 ohm --> 0.1 uF --> [transmission line] --> shunt 50 ohms (R472) --> 0.1 uF (C472).
- The cap at output of X3 prevents DC grounding the VCXO output. The 100 ohms and 50 ohms make a voltage divider to reduce 3.3 V to an acceptable level. To left of transmission line, place close to VCXO, to right of VCXO, place close to LMK IC.
For frequencies greater than 500 MHz I suggest a 3 dB pad for CLKin1. R206 naturally goes close to LMK IC.
Loop Filters
Loop filter 1, R463 and cap go close to VCXO input. Other I place closer to LMK IC output (convert current to voltage).
Loop filter 2, there is no value for R460/C441/R461/C442 unless an external VCO is being used. As I see no external VCO being used, the 3rd and 4th pole are integrated. I suggest you remove these components. Please remaining filter components near LMK.
I did not not check values of loop filters as I don't have the programming info of LMK or VCXO tuning gain (although I expect I could look this up in datasheet).
Outputs:
If AC coupled, LVPECL outputs should have emitter resistors placed to ground. I suggest 240 ohm. Otherwise some other appropriate LVPECL termination can be used. I don't see either.
If AC coupling LVDS/HSDS, place a 560 ohm shut resistor at output close to LMK IC. On LMK EVM, the 560 ohm is located in a poor place far from IC.
73,
Timothy
Hi Timothy,
I use WQFN package in LMK04821NKDT component. My customer ask about the rate between the die size and the package size. He said that if the rate is lower than 30%, the reliability of the chip is high.
Can you please tell the rate?
Thanks,
Shlomi