Hello,
I am looking for a clock generator in order to synchronize sensors in a network. My main task is that clock generator's output clocks should be as synchronous as possible, in the sense that they should not drift one with another.
My synchronization scheme has a clock generator board, which provides 20 synchronized 8.192 MHz clock outputs (these numbers are still to be confirmed). Each of these outputs needs to be carried to a different sensors board. Each board drives 4 ADCs and an RTCC, all still synchronized with the same clock.
My idea is to use a dual level scheme for the clock generator board, and a single clock generator for the sensors boards. I am now about to test CDCE706, of which I bought a few evaluation kits. it seems to be a good solution, but I have doubts about its jitter, which can reach 180 ps according to the data sheet, and it is not clear to me whether this can or cannot influence output drift.
Can you please give an advice on how I can evaluate the drift on the clock generator outputs, so that I can choose the best option?
Thanks in advance,
Stefano