Part Number: NE555
Other Parts Discussed in Thread: TLC555
Hi ,
My customer is using NE555 for 50% duty generation.
The circuit is attached. ---Vs=12V, Reset pin is pulled up to 12V, control is floating, 33k frequency(R=12k, C=1.8nF)
The disch pin output is as expected, while the output pin has 53% duty (3% ahead the disch voltage jump high).
You can check the waveform as below.
---The first question: Could you let me know what the possible reason for the unexpected 3% duty and how to remove it?
And, even for the disch pin, the duty is not 49% (not 50%). In our customer's application, we need a precise 50% duty cycle(49.75%-50.25% duty range) .
---The second question: The RC charging and discharging time should be the same, why the duty is not a good "50%"?
---The third question: What can we do to improve it basing on NE555 circuit? we can re-design the circuit?
---The fourth question: If 555 circuit can't make sure the good "50%", can you suggest a simple/low cost circuit if you have?
Thanks a lot.